Issue
Which model of UPS Network Management Card is supported in my UPS?
Product Line
- UPS Network Management Card for Easy UPS Online - AP9544
- UPS Network Management Card for Easy UPS, 3-Phase - AP9547
- UPS Network Management Card 3 - AP9640, AP9641, AP9643
- UPS Network Management Card 4 - AP9644
- UPS Network Management Card 2 - AP9630/30CH, AP9631/31CH, AP9635/35CH
- UPS Network Management Card 1 - AP9617, AP9618, AP9619
- UPS Web/SNMP Card - AP9606
Environment
- All firmware versions (unless otherwise specified)
- All serial numbers
Cause
This compatibility chart has been created for reference.
Resolution
Please refer to the table below.
Note: Some of these management cards are older and discontinued. This means while there may be some compatibility between current UPS models and discontinued management cards, support for new device features or management card features and bug fixes will only be available with the current generation of Network Management Card for your device. Current generation Network Management Cards purchased on their own will ship with the SUMX application file, for use with the Smart-UPS family. Firmware files for use in other UPS systems can be found here: http://www.apc.com/us/en/tools/download/ (Filter by Software/Firmware and choose "Firmware Upgrade")
Network Management Card Model(s) | UPS Model | Note(s) |
AP9547 (NMC3) |
| AP9547 does not support Easy UPS 3-Phase Modular. |
AP9544 (NMC3) |
| An alternate bracket is included in the box with the NMC card and must be screwed to the NMC before it can be inserted into the UPS device’s SmartSlot. This is applicable to below UPS models only: o SRV1KA o SRV1KA-TW o SRVPM6KRI o SRVPM6KRI-TW o SRVPM6KRIL o SRVPM6KRIL-TW o SRVSPM6KRI o SRV15KUXI-IN o SRV20KUXI-IN o SRVPM6KRILPK o SRV1KA-CA o SRV5KL-IN o SRV6KL-IN o SRV5KUXI-IN o SRV6KUXI-IN o SRV10KUXI-IN o SRVPM5KRI o SRVSPM5KRI o SRVSPM5KRIL o SRVPM10KRIL-IN o SRVPM10KRI o SRVSPM10KRI |
AP9640, AP9641, AP9643 (NMC3) |
|
|
AP9644 (NMC4) |
| Notes:
|
AP9630/30CH, AP9631/31CH (NMC2) |
|
|
AP9630/30CH, AP9631/31CH, AP9635/35CH (NMC2) |
|
|
AP9635/35CH (NMC2) |
|
|
G5K9635CH (NMC2) |
|
|
G9K9635CH (NMC2) |
|
|
AP9617, AP9618, AP9619 (NMC1) |
|
**Note: This add-on option is only able to monitor the UPS, and not any power distribution. The embedded NMC within the UPS must be used to monitor any power distribution. |
AP9606 |
| |
|
|
|
0G-9354 W0G-9354 (spare part) 0G-9354A 0J-0G-9354A (spare part) |
|
|
Note: Certain features are limited by application.
Released for:Schneider Electric India